N5244A/AS/B, N5245A/AS/B/BC, and N5247A/AS/B/BC with Option 029/E29
|
|
Before running this test, certain settings must be set in TME and the PNA. For TME:Be sure that For the PNA:Enable power sensor setting when using USB power sensor. |
This test takes advantage of the noise calibration available in the PNA firmware which characterizes the “noise parameters” of the noise receiver (similar to how a standard S-parameter cal characterizes the “error terms” of the receiver). A new type of calibration, one which utilizes a power sensor calibration (instead of using a noise source), has been implemented into the 50 GHz noise calibration and this calibration calculates error various noise parameters directly related to the noise figure of the receiver.
Thus, the test procedure for determining the noise figure contains two parts. The first part performs a noise (power meter) calibration and the second part reads the noise parameters resulting from this calibration and calculates the noise figure.
For the measurement part of this test (Normal Variant), the PNA will control the power meter. Therefore the operator will need to switch the power meter's GPIB connection from the main bus to the PNA's controller. Follow the steps in the Connection Setups section below.
For troubleshooting help, see Receiver Noise Figure Troubleshooting.
|
Test Equipment1 |
Recommended Model |
Alternate Model |
|
Power meter2 |
N1914B
|
N1914A |
|
Power sensor |
N8487A |
N8487A CFT |
|
Power sensor3 |
U8488A |
U8487A |
|
Calibration kit |
See selection tables below. |
|
|
|
|
|
|
Calibration Kits for |
|||
|
|
ECal Modules |
Mechanical3 |
|
|
Test Plan Variants |
N4693D2 Options 0DC, M0F N4693-61001 |
N4693-60001 |
85056A |
|
Factory Recommended |
X |
X |
X |
|
Normal |
|
X |
X |
|
|
Calibration Kits for |
|||
|
|
ECal Modules |
Mechanical3 |
|
|
Test Plan Variants |
N4694D2 Options 0DC, M0F |
N4694-60001 |
85058B |
|
Factory Recommended |
X |
X |
X |
|
Normal |
|
X |
X |
|
|
|
Due to the complexity of the PNA family of analyzers, the following notes apply to illustrations in the PNA Help:
|
For the measurement part of this test, the PNA will control the power meter. Therefore the operator will need to switch the power meter's GPIB connection from the main bus to the PNA's controller. There are two different GPIB ports on the rear of the PNA: GPIB(0) CONTROLLER and GPIB(1) TALKER/LISTENER. It is important to make the correct connections to the appropriate GPIB port as detailed in the instructions below.
The illustrations below show details of the GPIB connections of the power meter and the UUT. After the power sensor calibration, the UUT will directly control the power meter through the GPIB cable. In order for this to occur, follow the steps below.
Make sure that power meter's GPIB cable is only connected to the GPIB(0) CONTROLLER of the UUT and that the UUT's GPIB(1) TALKER/LISTENER is connected to the GPIB bus of the PC.
From the Power Sensor window, press OK.
If the GPIB and power sensor connections are correct, the test will proceed with the power measurement. If something is not correct, an error message such as Unable to recognize the power meter... will be displayed. Review the connection steps above.
|
|
Because of the variations possible with mechanical calibration setups, illustrations in TME and the Help will only show ECal setups. |