The test equipment that is required for performance verification is different for each PNA-L/X model family.
Select from the following list:
3.5 mm Connector Required Equipment
N5230A Options 02x, 12x, 14x, 22x, 24x
N5230C Options 02x, 12x, 14x, 22x, 24x
N5241A/AS, N5242A/AS, N5242AH85, N5249A/AS
N5241B/BC, N5242B, N5249B
N5221A/AS, N5222A/AS
N5221B, N5222B
N5231A/AS, N5232A/AS, N5239A/AS
N5231B, N5232B, N5239B
2.4 mm Connector Required Equipment
N5230A Options 42x, 52x
N5230C Options 42x, 52x
N5244A/AS, N5245A/AS
N5244B, N5245B/BC
N5224A/AS, N5225A/AS
N5224B, N5225B
N5234A/AS, N5235A/AS
N5234B, N5235B
1.85 mm Connector Required Equipment
N5247A/AS, N5227A/AS
N5247B/BC, N5227B
1 mm Connector Required Equipment
N5290A, N5291A
For a list of equipment required for a specific test, see the applicable test description in the Performance Tests section.
|
|
Equipment Lists for Test StationsGenerally, a single piece of equipment should not be entered multiple places in the equipment list for a given test station under TME. For instance, when a test station requires two power-sensor cables, two separate cables must be used. Mechanical calibration kits are an exception to this rule. When a test station lists two calibration kits, a single mechanical calibration kit may be used. |