|
|
|
Review the General Troubleshooting recommendations before proceeding with this section.
On the PNA, go to Utility > System > System Setup > Preferences. Ensure that this setting is NOT selected: Marker: Coupling controls on/off state of markers.
Be sure that
Pause on test point fail is not selected for this test.
This troubleshooting procedure assumes the PNA successfully passes the Noise Floor test.
If a phase lock lost error occurs during the test, it may cause the test to fail. Phase lock problems should be fixed before further troubleshooting. When a test fails on the N5247A PNA-X or is in an indeterminate state, make sure all the connectors are clean and torque all connections. If the test fails or is in an indeterminate state, rerun the test.
There are no adjustments for an analyzer which fails the Dynamic Accuracy Performance Test.
Refer to the appropriate PNA-X service guide for specific troubleshooting suggestions and replacement procedures.