Dynamic Accuracy Performance Test Overview
|
|
-
Dynamic Accuracy of a receiver consists of three regions: Compression, Linear, and Noise & Crosstalk. Measurements below -60 dBm are simply measuring noise variability in the Noise & Crosstalk region rather than the true linearity of the receiver! Since the receiver is linear by design at these levels, there is no need to measure linearity below this threshold. Making measurements above this threshold and below the compression region are sufficient to warrant linearity performance of a receiver.
-
Before starting this test, certain settings on the PNA should be verified. If it was necessary to change the settings, return the PNA to its previous state after the test is completed.
To verify the settings, go to: Utility > System > System Setup > Preferences
-
Be sure that Pause on test point fail is not selected for this test.
|
Test Plan Variants and Solution Choices
There are two test plan variants available: Factory Recommended Variant and Normal Variant. For the Normal Variant test plan (depending on model number), there are also two solution choices available: Preferred and Alternate.
Equipment and connection setups will differ depending on the variant and solution. For more information about test plan variants, refer to the Test Plan Variants topic. For more information about the two solutions available in the Normal Variant test plan, go to the Dynamic Accuracy Normal Variant Overview page.
Equipment and Connection Setups
For equipment and connection setups, select from the links below for the appropriate test plan variant: