Review the General Troubleshooting recommendations before proceeding with this section.
This test uses data from the Maximum Output Power test and the Noise Floor test. If the System Dynamic Range test should fail, re-run the Maximum Output Power test and the Noise Floor test. And then re-run the System Dynamic Range test.
Be sure that
Pause on test point fail is not selected for this test.