|
|
|
This procedure performs two separate adjustments on the NA source. The first is an adjustment of the default maximum source power level to prevent severe compression in the reflection or test receiver channels when the default maximum power level is selected. The second adds additional attenuation to lower frequency bands to prevent an IF Overload (actually an IF over-range condition at the ADC.).
There are two independent steps to this adjustment. First, Maximum Power is set for the first thirteen bands. This currently covers frequencies up to ~625 MHz. Second, the maximum power is further adjusted in the first four bands (up to ~20 MHz) to prevent the IF signal level from getting so large that it causes the ADC to overflow when converting maximum power level signals. Before the adjustment routine is allowed to begin, the DUT operating temperature is checked to be sure that the internal temperatures have reached a point where the DUT is stable with respect to normal ambient room temperatures.
|
Related test: |
|
Test Equipment |
Recommended Model Number |
|---|---|
|
Power Meter |
N1914A |
|
Power Sensor |
E9304A Opt H20 |
|
Power Sensor Cable |
11730A |
|
|
The following notes apply to illustrations in the FieldFox Help:
|