Relative power measurements use a receiver to measure the power at every step in the step attenuator relative to the step used during the Synthesizer Output Power Adjustment.
|
Test Equipment |
Recommended Models1 |
|
Spectrum analyzer |
N9030A |
|
Attenuator, 6 dB Fixed |
8493C Opt. 006 |
|
Adapter, 3.5 mm (f) to 2.4 mm (f) |
11901B |
|
Cable, 3.5 mm (m) to 3.5 mm (m) |
11500E |
|
Frequency reference module |
M9300A |
|
|
|
|
For procedures that apply to multiple ports, illustrations will show the setup on only one test port. |