Keysight 89600 VSA .NET API
AMUnit Property
See Also 
Agilent.SA.Vsa.AnalogDemod.Interfaces Assembly > Agilent.SA.Vsa.AnalogDemod Namespace > AnalogDemodChannel Class : AMUnit Property


Glossary Item Box

Gets or sets the AM demod units.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property AMUnit As AnalogDemodAMUnitType
C# 
public abstract AnalogDemodAMUnitType AMUnit {get; set;}
C++/CLI 
public:
abstract property AnalogDemodAMUnitType AMUnit {
   AnalogDemodAMUnitType get();
   void set (    AnalogDemodAMUnitType value);
}

Remarks

You can select the AM modulation index results to be calculated in % or AM units. The AMUnit feature is applicable only to AnalogDemodType.AM analog demodulation.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also