| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Sub MoveTo( _ ByVal indexFrom As Integer, _ ByVal indexTo As Integer _ ) | |
Parameters
- indexFrom
- Current or "old" index of the constellation state.
- indexTo
- Index (position) the constellation state is to be moved to.
The indexes indexFrom and indexTo represent positions as they exist before moving the ConstellationState. They must be in the range of 0 to Count-1.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.00