Keysight 89600 VSA .NET API
ConstellationStyle Enumeration
See Also 
Agilent.SA.Vsa.CustomIQ.Interfaces Assembly > Agilent.SA.Vsa.CustomIQ Namespace : ConstellationStyle Enumeration


Glossary Item Box

Presets for use as a starting point in creating a constellation definition.

Syntax

Visual Basic (Declaration) 
Public Enum ConstellationStyle 
   Inherits System.Enum
C# 
public enum ConstellationStyle : System.Enum 
C++/CLI 
public enum class ConstellationStyle : public System.Enum 

Members

MemberDescriptionMinimum SW Version‡
CrossQamCross QAM modulation. Cross QAM constellation presets are supported for the following number of constellation states: 32, 128, 512, 2048, 8192, 32768.30.40
PskUniform PSK modulation. PSK constellation presets are supported for two or more constellation states.—
SquareQamSquare QAM modulation. Square QAM constellation presets are supported for the following number of constellation states: 2, 4, 16, 64, 256, 1024, 4096, 16384.—
‡ This is the minimum 89600 VSA software version level needed to use this enum member.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.00

See Also