Preset the constellation definition.
Syntax
Parameters
- style
- Determines the pre-defined constellation style to use for the setting the constellation definition.
- numberOfStates
- The number of constellation states to use for the created constellation. The valid values for this parameter depend upon the selected ConstellationStyle.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 18.00
See Also