Keysight 89600 VSA .NET API
Export Method
See Also 
Agilent.SA.Vsa.CustomIQ.Interfaces Assembly > Agilent.SA.Vsa.CustomIQ Namespace > Constellation Class : Export Method


Glossary Item Box

Export constellation states to a string representation.

Syntax

Visual Basic (Declaration) 
Public Overridable Function Export() As String
C# 
public virtual string Export()
C++/CLI 
public:
virtual String^ Export(); 

Return Value

String containing constellation state data in CSV format

Remarks

Returns a CSV format string with each line containing: Index,Real,Imaginary,Symbol(Hex). This is the same format used by Keysight N7608B Signal Studio for Custom Modulation.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 30.40

See Also