Keysight 89600 VSA .NET API
Constellation Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.CustomIQ.Interfaces Assembly > Agilent.SA.Vsa.CustomIQ Namespace : Constellation Class

Glossary Item Box

The following tables list the members exposed by Constellation.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyConstellationStatesGets the constellation states.  18.00
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyMagnitudeRmsGets the RMS of the magnitude of the reference constellation states.  18.00
Public PropertyNameGets or sets the name of the constellation. The name must be unique.  18.00
Public PropertySymbolMapSourceGets or sets the source for deriving the used symbol map for the Constellation.  18.00
Public PropertySymmetryAngleGets the minimum rotation angle in degrees for an equivalent constellation  18.00
Public PropertyValidationFailureDescriptionGets a description of any validation failure condition from the most recent call to Validate.  18.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCopyFromReplaces the current contents of this constellation with content copied from the selected source constellation.  18.00
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodExportExport constellation states to a string representation.  30.40
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodImportImport constellation states from a string representation.  30.40
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodNormalizeNormalize the current constellation definition to a specified reference level.  18.00
Public MethodNormalizeRmsNormalize the current constellation definition to an RMS magnitude of 1.0.  18.00
Public MethodPresetPreset the constellation definition.  18.00
Public MethodRecallRecall constellation states from a text file generated by Keysight N7608B Signal Studio for Custom Modulation.  24.20
Public MethodRotateRotate the current constellation definition by the specified angle (in degrees).  18.00
Public MethodSaveSave constellation states to a text file that can be used by Keysight N7608B Signal Studio for Custom Modulation.  30.40
Public MethodValidateValidate the current constellation definition and return characteristic information.  18.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also