| Visual Basic (Declaration) | |
|---|---|
Public Overridable Sub Import( _ ByVal constellationData As String _ ) | |
| C# | |
|---|---|
public virtual void Import( string constellationData ) | |
| C++/CLI | |
|---|---|
public: virtual void Import( String^ constellationData ) | |
Parameters
- constellationData
- String containing constellation state data in CSV format
The string format is CSV with each line containing: Index,Real,Imaginary,Symbol(Hex). This is the same format used by Keysight N7608B Signal Studio for Custom Modulation.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 30.40