Keysight 89600 VSA .NET API
EqualizerMode Property
See Also 
Agilent.SA.Vsa.CustomIQ.Interfaces Assembly > Agilent.SA.Vsa.CustomIQ Namespace > MeasurementExtension Class : EqualizerMode Property


Glossary Item Box

Gets or sets the run mode of the Adaptive Equalizer.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property EqualizerMode As EqualizerMode
C# 
public abstract EqualizerMode EqualizerMode {get; set;}
C++/CLI 
public:
abstract property EqualizerMode EqualizerMode {
   EqualizerMode get();
   void set (    EqualizerMode value);
}

Remarks

Determine whether the adaptive equalizer of the digital demodulation is currently running. To use the adaptive equalizer, it must be turned on (IsEqualized set to true) and EqualizerMode must be set to EqualizerMode.Run. You can set the equalizer to stop adapting and hold its current filter by setting EqualizerMode to EqualizerMode.Hold. You can equalize to start over from its initial state by calling EqualizerReset. For more information, see Digital Demodulation "About Adaptive Equalization" topic in the VSA Application help.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 18.00

See Also