Keysight 89600 VSA .NET API
DisplayedCarrierIndex Property
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > CarrierAggregation Class : DisplayedCarrierIndex Property


Glossary Item Box

Gets or sets the index of the carrier shown in Demod traces that are not fixed to a specific ComponentCarrier.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property DisplayedCarrierIndex As Integer
C# 
public abstract int DisplayedCarrierIndex {get; set;}
C++/CLI 
public:
abstract property int DisplayedCarrierIndex {
   int get();
   void set (    int value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also