Gets the list of indexes of
Agilent.SA.Vsa.Input.MeasurementChannels assigned to this
ComponentCarrier.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Function GetAssignedMeasurementChannelIndexes() As Integer() |
| C# | |
|---|
public abstract int[] GetAssignedMeasurementChannelIndexes() |
| C++/CLI | |
|---|
public:
abstract array<int>^ GetAssignedMeasurementChannelIndexes(); |
Return Value
Zero-based measurement channel indexes.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
See Also