The following tables list the members exposed by ComponentCarrier.
| Name | Description | Minimum SW Version | |
|---|---|---|---|
![]() | AllDataStreamsActive | Gets or sets a value indicating whether all data streams are active for this component carrier. | — |
![]() | AntennaDetectionThreshold | Gets or sets the antenna-detection threshold (dB) for this component carrier. | — |
![]() | CenterFrequency | Gets or sets the absolute center frequency in Hz. Setting this adjusts OffsetFromReferenceFrequency accordingly. | — |
![]() | Enabled | Gets or sets a value indicating whether this ComponentCarrier is analyzed and shown in trace results. | — |
![]() | EnableHalfSubcarrierShift | Gets or sets a value indicating whether a half-subcarrier shift is applied for this component carrier. | — |
![]() | EqualizerMode | Gets or sets the equalizer mode for this component carrier. | — |
![]() | EqualizerSmoothingFilterLength | Gets or sets the equalizer smoothing filter length for this component carrier. | — |
![]() | EqualizerSmoothingMode | Gets or sets the equalizer smoothing mode for this component carrier. | — |
![]() | ExtendedFrequencyLockRangeWidth | Gets or sets the extended frequency-lock-range width for this component carrier. | — |
![]() | FbmcSettings | Gets the FBMC settings for this component carrier. | — |
![]() | FftLength | Gets or sets the FFT length used to demodulate this component carrier. | — |
![]() | FrameCreationUtility | Gets the frame-creation utility (Frame Definition authoring and Apply) for this component carrier. | — |
![]() | GuardInterval | Gets or sets the guard interval (fraction of the FFT length) for this component carrier. | — |
![]() | GuardIntervalRepeatIndex | Gets or sets the guard-interval repeat index for this component carrier. | — |
![]() | GuardLowerSubcarriers | Gets or sets the number of lower guard subcarriers for this component carrier. | — |
![]() | GuardUpperSubcarriers | Gets or sets the number of upper guard subcarriers for this component carrier. | — |
![]() | InitialEqualizerMode | Gets or sets the initial-equalizer mode for this component carrier. | — |
![]() | InitialEqualizerSymbols | Gets or sets the number of initial-equalizer symbols for this component carrier. | — |
![]() | IsDisposed | Gets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | IsEqualizerUseData | Gets or sets a value indicating whether the equalizer uses data subcarriers for this component carrier. | — |
![]() | IsEqualizerUseDCPilot | Gets or sets a value indicating whether the equalizer uses the DC pilot for this component carrier. | — |
![]() | IsEqualizerUsePilots | Gets or sets a value indicating whether the equalizer uses pilots for this component carrier. | — |
![]() | IsEqualizerUsePreamble | Gets or sets a value indicating whether the equalizer uses the preamble for this component carrier. | — |
![]() | IsEvmNormalizeByReference | Gets or sets a value indicating whether EVM is normalized by the reference for this component carrier. | — |
![]() | IsExtendedFrequencyLockRange | Gets or sets a value indicating whether the extended frequency lock range is enabled for this component carrier. | — |
![]() | IsFrequencyMirrored | Gets or sets a value indicating whether the spectrum is frequency-mirrored for this component carrier. | — |
![]() | IsOfdmErrorVectorBeforeIdftDespread | Gets or sets a value indicating whether the OFDM error vector is computed before IDFT despread for this component carrier. | — |
![]() | IsPilotDefinedInTimeDomain | Gets or sets a value indicating whether the pilot is defined in the time domain for this component carrier. | — |
![]() | IsPulsedSignal | Gets or sets a value indicating whether the signal is treated as pulsed for this component carrier. | — |
![]() | IsPulseSearchEnabled | Gets or sets a value indicating whether pulse search is enabled for this component carrier. | — |
![]() | IsPulseSearchThresholdAutomatic | Gets or sets a value indicating whether the pulse-search threshold is automatic for this component carrier. | — |
![]() | IsSampleClockCompensated | Gets or sets a value indicating whether the sample clock is compensated for this component carrier. | — |
![]() | IsTrackAmplitude | Gets or sets a value indicating whether amplitude tracking is enabled for this component carrier. | — |
![]() | IsTrackDataSubcarriers | Gets or sets a value indicating whether data-subcarrier tracking is enabled for this component carrier. | — |
![]() | IsTrackPhase | Gets or sets a value indicating whether phase tracking is enabled for this component carrier. | — |
![]() | IsTrackTiming | Gets or sets a value indicating whether timing tracking is enabled for this component carrier. | — |
![]() | MeasurementInterval | Gets or sets the measurement interval (symbols) for this component carrier. | — |
![]() | MeasurementOffset | Gets or sets the measurement offset (symbols) for this component carrier. | — |
![]() | ModulationScheme | Gets or sets the modulation scheme for this component carrier. | — |
![]() | MulticarrierFilter | Gets the multicarrier filter settings for this component carrier. | — |
![]() | MultipleAccessScheme | Gets or sets the multiple-access scheme for this component carrier. | — |
![]() | Name | Gets the component carrier name (for example, "CC0"). | — |
![]() | NamePerUser | Gets or sets the comma-separated list of names for each user ID for this component carrier. | — |
![]() | NomaSettings | Gets the NOMA settings for this component carrier. | — |
![]() | OfdmSystemSampleFrequency | Gets or sets the OFDM system sample frequency (Hz) for this component carrier. | — |
![]() | OffsetFromReferenceFrequency | Gets or sets the center frequency offset in Hz from ReferenceFrequency (CenterFrequency = ReferenceFrequency + OffsetFromReferenceFrequency). | — |
![]() | PulseSearchThreshold | Gets or sets the pulse-search threshold (dB) for this component carrier. | — |
![]() | ReferenceConstellationValuesAutoDetected | Gets or sets a value indicating whether reference constellation values are auto-detected for this component carrier. | — |
![]() | ResourceInterface | Gets or sets the resource interface for this component carrier. | — |
![]() | ResourceRepeatIndex | Gets or sets the resource repeat index for this component carrier. | — |
![]() | ResultLength | Gets or sets the result length (symbols) for this component carrier. | — |
![]() | ResultLengthSelection | Gets or sets the result-length selection mode for this component carrier. | — |
![]() | ScmaSettings | Gets the SCMA settings for this component carrier. | — |
![]() | SearchLength | Gets or sets the search length (seconds) for this component carrier. | — |
![]() | SymbolPhaseCompensationFrequency | Gets or sets the symbol-phase-compensation frequency (Hz) for this component carrier. | — |
![]() | SymbolPhaseCompensationSource | Gets or sets the symbol-phase-compensation source for this component carrier. | — |
![]() | SymbolTimeAdjustment | Gets or sets the symbol time adjustment (%) for this component carrier. | — |
![]() | SynchronizationAntennaPortIndex | Gets or sets the synchronization antenna port index for this component carrier. | — |
![]() | SynchronizationMeasurementChannelIndex | Gets or sets the synchronization measurement channel index for this component carrier. | — |
![]() | SynchronizationMode | Gets or sets the synchronization mode for this component carrier. | — |
![]() | SynchronizationReferenceInterval | Gets or sets the synchronization reference interval for this component carrier. | — |
![]() | SynchronizationReferenceOffset | Gets or sets the synchronization reference offset for this component carrier. | — |
![]() | SynchronizationRegionSelection | Gets or sets the synchronization region selection for this component carrier. | — |
![]() | SynchronizationSearchInterval | Gets or sets the synchronization search interval for this component carrier. | — |
![]() | SynchronizationSearchOffset | Gets or sets the synchronization search offset for this component carrier. | — |
![]() | TimeGapsRepeatIndex | Gets or sets the time-gaps repeat index for this component carrier. | — |
![]() | TransmitterAntennas | Gets or sets the number of transmitter antennas for this component carrier. | — |
![]() | TransmitterWindowBeta | Gets or sets the transmitter window beta for this component carrier. | — |
![]() | UnknownPilotBoostLevel | Gets or sets the unknown-pilot boost level for this component carrier. | — |
| ‡ This is the minimum 89600 VSA software version level needed to use this member. | |||
| Name | Description | Minimum SW Version | |
|---|---|---|---|
![]() | CopySettingsFrom | Overloaded. Copies all settings from the specified ComponentCarrier, including its assigned measurement channels, OffsetFromReferenceFrequency and Enabled state. | — |
![]() | CreateObjRef | Creates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject) | — |
![]() | ForceRebuildKeyMap | This method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | GetActivePortsPerAllocation | Gets the active ports per allocation for this component carrier. | — |
![]() | GetAssignedMeasurementChannelIndexes | Gets the list of indexes of Agilent.SA.Vsa.Input.MeasurementChannels assigned to this ComponentCarrier. | — |
![]() | GetCdmGroupSubcarrierCountPerFramePart | Gets the CDM-group subcarrier count per frame part for this component carrier. | — |
![]() | GetCdmGroupSubcarrierCountPerUser | Gets the CDM-group subcarrier count per user for this component carrier. | — |
![]() | GetCdmGroupSymbolCountPerFramePart | Gets the CDM-group symbol count per frame part for this component carrier. | — |
![]() | GetCdmGroupSymbolCountPerUser | Gets the CDM-group symbol count per user for this component carrier. | — |
![]() | GetCyclicSuffixPerSymbol | Gets the cyclic suffix per symbol for this component carrier. | — |
![]() | GetFramePartIdPerAllocation | Gets the frame-part ID per allocation for this component carrier. | — |
![]() | GetGuardIntervalPerSymbol | Gets the guard interval per symbol for this component carrier. | — |
![]() | GetLifetimeService | Retrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject) | — |
![]() | GetModulationPerAllocation | Gets the modulation per allocation for this component carrier. | — |
![]() | GetPilotValues | Gets the pilot values for this component carrier. | — |
![]() | GetPowerBoostLevelPerAllocation | Gets the power boost level per allocation for this component carrier. | — |
![]() | GetPowerBoostLevelPerUser | Gets the per-user power boost levels for this component carrier. | — |
![]() | GetPreambleValues | Gets the preamble values for this component carrier. | — |
![]() | GetQamIdentifierPowerBoostLevels | Gets the QAM identifier power boost levels for this component carrier. | — |
![]() | GetQamIdentifiers | Gets the QAM identifiers for this component carrier. | — |
![]() | GetQamLevels | Gets the QAM levels for this component carrier. | — |
![]() | GetReferenceConstellationValues | Gets the reference constellation values for this component carrier. | — |
![]() | GetReferenceDataValues | Gets the reference data values for this component carrier. | — |
![]() | GetResourceAllocations | Gets the resource allocations for this component carrier. | — |
![]() | GetResourceMap | Gets the resource map for this component carrier. | — |
![]() | GetResourceModulations | Gets the resource modulation for this component carrier. | — |
![]() | GetResourceTypePerAllocation | Gets the resource type per allocation for this component carrier. | — |
![]() | GetTimeGapPerSymbol | Gets the time gap before each OFDM symbol for this component carrier, defined in samples at the OFDM system sample frequency. | — |
![]() | GetUserIdPerAllocation | Gets the user ID per allocation for this component carrier. | — |
![]() | InitializeLifetimeService | Obtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | Preset | Presets this component carrier to the specified standard. | — |
![]() | SetActivePortsPerAllocation | Sets the active ports per allocation for this component carrier. | — |
![]() | SetAssignedMeasurementChannels | Sets the list of Agilent.SA.Vsa.Input.MeasurementChannels assigned to this ComponentCarrier. | — |
![]() | SetCdmGroupSubcarrierCountPerFramePart | Sets the CDM-group subcarrier count per frame part for this component carrier. | — |
![]() | SetCdmGroupSubcarrierCountPerUser | Sets the CDM-group subcarrier count per user for this component carrier. | — |
![]() | SetCdmGroupSymbolCountPerFramePart | Sets the CDM-group symbol count per frame part for this component carrier. | — |
![]() | SetCdmGroupSymbolCountPerUser | Sets the CDM-group symbol count per user for this component carrier. | — |
![]() | SetCyclicSuffixPerSymbol | Sets the cyclic suffix per symbol for this component carrier. | — |
![]() | SetFramePartIdPerAllocation | Sets the frame-part ID per allocation for this component carrier. | — |
![]() | SetGuardIntervalPerSymbol | Sets the guard interval per symbol for this component carrier. | — |
![]() | SetModulationPerAllocation | Sets the modulation per allocation for this component carrier. | — |
![]() | SetPilotValues | Sets the pilot values for this component carrier. | — |
![]() | SetPowerBoostLevelPerAllocation | Sets the power boost level per allocation for this component carrier. | — |
![]() | SetPowerBoostLevelPerUser | Sets the per-user power boost levels for this component carrier. | — |
![]() | SetPreambleValues | Sets the preamble values for this component carrier. | — |
![]() | SetQamIdentifierPowerBoostLevels | Sets the QAM identifier power boost levels for this component carrier. | — |
![]() | SetQamIdentifiers | Sets the QAM identifiers for this component carrier. | — |
![]() | SetQamLevels | Sets the QAM levels for this component carrier. | — |
![]() | SetReferenceConstellationValues | Sets the reference constellation values for this component carrier. | — |
![]() | SetReferenceDataValues | Sets the reference data values for this component carrier. | — |
![]() | SetResourceAllocations | Sets the resource allocations for this component carrier. | — |
![]() | SetResourceMap | Sets the resource map for this component carrier. | — |
![]() | SetResourceModulations | Sets the resource modulation for this component carrier. | — |
![]() | SetResourceTypePerAllocation | Sets the resource type per allocation for this component carrier. | — |
![]() | SetTimeGapPerSymbol | Sets the time gap before each OFDM symbol for this component carrier, defined in samples at the OFDM system sample frequency. | — |
![]() | SetUserIdPerAllocation | Sets the user ID per allocation for this component carrier. | — |
| ‡ This is the minimum 89600 VSA software version level needed to use this member. | |||
| Name | Description | Minimum SW Version | |
|---|---|---|---|
![]() | PropertyChanged | Occurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | PropertyInfoChanged | Occurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | RemotePropertyChanged | Occurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | — |
![]() | RemotePropertyInfoChanged | Occurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject) | 14.00 |
| ‡ This is the minimum 89600 VSA software version level needed to use this member. | |||