Keysight 89600 VSA .NET API
GetResourceTypePerAllocation Method
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > ComponentCarrier Class : GetResourceTypePerAllocation Method


Glossary Item Box

Gets the resource type per allocation for this component carrier.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function GetResourceTypePerAllocation() As Integer()
C# 
public abstract int[] GetResourceTypePerAllocation()
C++/CLI 
public:
abstract array<int>^ GetResourceTypePerAllocation(); 

Return Value

The resource type per allocation.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also