Keysight 89600 VSA .NET API
SetResourceTypePerAllocation Method
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > ComponentCarrier Class : SetResourceTypePerAllocation Method


value
The resource type per allocation.

Glossary Item Box

Sets the resource type per allocation for this component carrier.

Syntax

Visual Basic (Declaration) 
Public MustOverride Sub SetResourceTypePerAllocation( _
   ByVal ParamArray value() As Integer _
) 
C# 
public abstract void SetResourceTypePerAllocation( 
   params int[] value
)
C++/CLI 
public:
abstract void SetResourceTypePerAllocation( 
   ... array<int>^ value
) 

Parameters

value
The resource type per allocation.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also