| Visual Basic (Declaration) | |
|---|---|
Public Overridable Sub SetTimeGapPerSymbol( _ ByVal ParamArray timeGapPerSymbol() As Single _ ) | |
| C# | |
|---|---|
public virtual void SetTimeGapPerSymbol( params float[] timeGapPerSymbol ) | |
| C++/CLI | |
|---|---|
public: virtual void SetTimeGapPerSymbol( ... array<float>^ timeGapPerSymbol ) | |
Parameters
- timeGapPerSymbol
- integer array, one value per symbol
If the array is empty (the default) then there are no time gaps in the signal. If the end of the array is reached, processing loops back to the symbol number specified by TimeGapsRepeatIndex. This is an array of floating-point values, but currently the values are always rounded to the nearest OFDM FFT sample.
When the ModulationScheme is set to ModulationScheme.Fbmc, this property is ignored.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00