| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property TimeGapsRepeatIndex As Integer | |
| C# | |
|---|---|
public virtual int TimeGapsRepeatIndex {get; set;} | |
Property Value
The default value is 0. The minimum value is zero.When using array set by SetTimeGapPerSymbol , the analyzer needs enough values for the ResultLength. If the array is shorter than that, the TimeGapsRepeatIndex specifies where to loop back to in the array after the end is reached.
The value is specified in terms of symbol number. As an example, a value of zero means that the analyzer loops back to the beginning of the array.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00