Gets the array of reference I/Q constellation values used when
ReferenceConstellationValuesAutoDetected is
false.
Syntax
| Visual Basic (Declaration) | |
|---|
Public Overridable Function GetReferenceConstellationValues() As Single() |
| C# | |
|---|
public virtual float[] GetReferenceConstellationValues() |
| C++/CLI | |
|---|
public:
virtual array<float>^ GetReferenceConstellationValues(); |
Return Value
interleaved I and Q values for each constellation point, first across subcarriers for an OFDM symbol, starting with the lowest subcarrier, then across OFDM symbols, and finally across streams. For multi-stream signals the per-stream blocks are concatenated stream-major (stream 0's complete subcarrier-by-symbol block first, then stream 1's, and so on), with every per-stream block the same length. The layout matches
SetReferenceConstellationValues.
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 31.00
See Also