Keysight 89600 VSA .NET API
PassBandwidth Property
See Also 
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace > MulticarrierFilter Class : PassBandwidth Property


Glossary Item Box

Gets or sets the two-sided filter pass bandwidth for multi-carrier filter, as a fraction of the OFDM system sample frequency.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property PassBandwidth As Double
C# 
public abstract double PassBandwidth {get; set;}
C++/CLI 
public:
abstract property double PassBandwidth {
   double get();
   void set (    double value);
}

Property Value

The default value is 0.8. The maximum value is 1.0, and the minimum is 0.0.

Remarks

This is used only when Selection is set to MulticarrierFilterSelection.WindowedSinc or MulticarrierFilterSelection.Remez. For WindowedSinc, this bandwidth is only used when IsWindowedSincLengthAutomatic is true.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.00

See Also