| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property WindowedSincLength As Integer | |
| C# | |
|---|---|
public abstract int WindowedSincLength {get; set;} | |
Property Value
The default value is 32 points. The maximum value is 1000, and the minimum is 1.This is used only when Selection is set to MulticarrierFilterSelection.WindowedSinc.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 21.00