Keysight 89600 VSA .NET API
MulticarrierFilter Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.CustomOfdm.Interfaces Assembly > Agilent.SA.Vsa.CustomOfdm Namespace : MulticarrierFilter Class

Glossary Item Box

The following tables list the members exposed by MulticarrierFilter.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyArbitraryCoefficientsGets or sets the multi-carrier filter coefficients.  21.00
Public PropertyArbitraryCoefficientsSampleRatioGets or sets the sample ratio of the arbitrary filter coefficients, relative to the OFDM system sample frequency.  21.00
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsWindowedSincLengthAutomaticGets or sets a value indicating whether the number of time-domain coefficients for the multi-carrier filter is automatically calculated.  21.00
Public PropertyPassBandwidthGets or sets the two-sided filter pass bandwidth for multi-carrier filter, as a fraction of the OFDM system sample frequency.  21.00
Public PropertyRemezAttenuationGets or sets the attenuation of the multi-carrier filter, in dB.  21.00
Public PropertyRemezRippleGets or sets the peak-to-peak pass-band ripple of the multi-carrier filter, in dB.  21.00
Public PropertySelectionGets or sets the method for selecting the multi-carrier filter.  21.00
Public PropertyTransitionBandwidthGets or sets the transition bandwidth for multi-carrier filter, as a fraction of the OFDM system sample frequency.  21.00
Public PropertyWindowedSincLengthGets or sets the multi-carrier filter time-domain coefficient length in points.  21.00
Public PropertyWindowedSincWindowGets or sets the window used when synthesizing the multi-carrier filter coefficients.  21.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also