Gets or sets the attenuation of the multi-carrier filter, in dB.
Syntax
| Visual Basic (Declaration) | |
|---|
Public MustOverride Property RemezAttenuation As Double |
| C# | |
|---|
public abstract double RemezAttenuation {get; set;} |
| C++/CLI | |
|---|
public:
abstract property double RemezAttenuation {
double get();
void set ( double value);
} |
Property Value
The default value is -60. The maximum value is 0, and the minimum is -300.
Remarks
Requirements
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA
Ver 21.00
See Also