| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property PreselectorBypass As Boolean | |
| C# | |
|---|---|
public abstract bool PreselectorBypass {get; set;} | |
The Microwave Preselector parameter allows you to select the microwave preselector and only applies to measurements above 3 GHz. This parameter is ignored if option 123 is not installed. The default value is to turn the preselector off (false).
false: The microwave preselector (YIG-tuned pre-selection filter) is bypassed for measurements above 3 GHz. This selection increases amplitude accuracy for wideband measurements however, at the expense of selectivity and image protection.
true: The microwave preselector (YIG-tuned pre-selection filter) is used for measurements above 3 GHz. This selection provides full image protection guarding against aliasing products.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)