Keysight 89600 VSA .NET API
InputExtension Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.HardwareExtensions.Core.Interfaces Assembly > Agilent.SA.Vsa.HardwareExtensions.Psa Namespace : InputExtension Class

Glossary Item Box

The following tables list the members exposed by InputExtension.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAcquisitionIndexGets the acquisition index that this input extension is a part of when using sequential input channel configurations. (Inherited from Agilent.SA.Vsa.InputExtension)25.00
Public PropertyADCDitherGets or sets a value indicating whether the ADC dither signal is on.  —
Public PropertyChannelsGets a reference to a collection of channel objects (one per physical channel) for custom input parameters that are per channel. This collection may be empty if no per channel custom input parameters are supported for the current hardware being used. (Inherited from Agilent.SA.Vsa.InputExtension)30.00
Public PropertyDisplayUpdatesGets or sets a value indicating whether display updates on the PSA instrument are on.  —
Public PropertyExternalTriggerLocationGets or sets which external trigger port to use  —
Public PropertyGroupIndexGets the index of the instrument group in the current hardware configuration that is associated with this input extension object (for the case when Agilent.SA.Vsa.Input.AcquisitionSequenceCount has a value of 1). When the Agilent.SA.Vsa.Input.AcquisitionSequenceCount has a value greater than 1 then this property is the index of the Agilent.SA.Vsa.InputExtension item within the Agilent.SA.Vsa.InputExtensionCollection. (Inherited from Agilent.SA.Vsa.InputExtension)—
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyLogicalInstrumentIndexGets the index of the logical instrument in the current hardware configuration that is associated with this input extension object. (Inherited from Agilent.SA.Vsa.InputExtension)30.00
Public PropertyPreselectorBypassGets or sets a value indicating whether the microwave preselector is bypassed.  —
Public PropertyUnlockFrontPanelGets or sets a value indicating whether the front panel of the PSA instrument is unlocked.  —
Public PropertyUserSCPIPresetGets or sets PSA setup commands that are not set by the 89601 software  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodGetParameterGets the value of the named parameter on the specified instrument type. (Inherited from Agilent.SA.Vsa.InputExtension)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodParameterNamesGets an array of strings representing the named parameters that can be configured on this hardware. (Inherited from Agilent.SA.Vsa.InputExtension)—
Public MethodSetParameterSets the named parameter on the specified instrument type to the value specified. (Inherited from Agilent.SA.Vsa.InputExtension)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also