Keysight 89600 VSA .NET API
ActualPreamplifier Property
See Also 
Agilent.SA.Vsa.HardwareExtensions.Core.Interfaces Assembly > Agilent.SA.Vsa.HardwareExtensions.XSeries Namespace > InputExtension Class : ActualPreamplifier Property


Glossary Item Box

Gets a value indicating what the actual preamplifier state is that is being used. Normally Preamplifier will be the actual state, except when RFGainAdjustmentAllowed is in the On or in the RFGainAdjustmentAllowed.Auto mode (and has chosen to use the On state) in which case when Preamplifier is set to Preamplifier.Off then Preamplifier.Adjusted may be the actual state.

Syntax

Visual Basic (Declaration) 
Public Overridable ReadOnly Property ActualPreamplifier As Preamplifier
C# 
public virtual Preamplifier ActualPreamplifier {get;}
C++/CLI 
public:
virtual property Preamplifier ActualPreamplifier {
   Preamplifier get();
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 30.25

See Also