| Visual Basic (Declaration) | |
|---|---|
Public Overloads Overridable Sub RecallSetup( _ ByVal fileName As String, _ ByVal append As Boolean, _ ByVal shareInput As Boolean, _ ByVal dataSourceValueToUse As DataSourceValueToUse _ ) | |
| C# | |
|---|---|
public virtual void RecallSetup( string fileName, bool append, bool shareInput, DataSourceValueToUse dataSourceValueToUse ) | |
| C++/CLI | |
|---|---|
public: virtual void RecallSetup( String^ fileName, bool append, bool shareInput, DataSourceValueToUse dataSourceValueToUse ) | |
Parameters
- fileName
- The name of the file to recall. Supported files include Keysight 89600 VSA Software setup files (.SETX extension) and Agilent 89601A setup files (.SET extension).
- append
- When 'true', the setup information in the specified file is appended to the existing setup. Otherwise, when 'false', the setup information in the file replaces the existing setup.
- shareInput
- This parameter is ignored unless append is true and the setup file being recalled contains only a single measurement. When both these conditions are true and shareInput is also 'true', the Measurement.IsShareEnabled property of the currently selected measurement and the measurement being recalled are both set to 'true', resulting in both measurements sharing the same analyzer or recording file.
- dataSourceValueToUse
- This parameter is ignored if both append and shareInput are true. This parameter specifies what data source will be used for the measurement setup. When DataSourceValueToUse.Recording or DataSourceValueToUse.Hardware is chosen, the data source is explicitly specified. When DataSourceValueToUse.FromSetupFile or DataSourceValueToUse.FromCurrentState is chosen, the data source is specified by the setup file or current measurement.
This method appends the setup information contained in the specified file to the existing setup if the append parameter is 'true'.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 29.00