Keysight 89600 VSA .NET API
BeginQuickCalibration Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Calibration Class : BeginQuickCalibration Method


Glossary Item Box

Starts a partial calibration of the input hardware.

Syntax

Visual Basic (Declaration) 
Public MustOverride Sub BeginQuickCalibration() 
C# 
public abstract void BeginQuickCalibration()
C++/CLI 
public:
abstract void BeginQuickCalibration(); 

Remarks

This method returns immediately (before the partial calibration is finished). Query Application.Measurements.SelectedItem.Status.Value and check the Vsa.Status.Calibrating bit to see when it is done.

A calibration is not performed if this function is called unless the active measurement's Input.DataFrom property is set to DataSource.Hardware.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also