Keysight 89600 VSA .NET API
ModeAuto Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Calibration Class : ModeAuto Property


Glossary Item Box

Gets or sets a value indicating whether the calibration mode is chosen automatically by the hardware. When on, the hardware selects the mode itself and Mode reflects the chosen mode.

Syntax

Visual Basic (Declaration) 
Public Overridable Property ModeAuto As Boolean
C# 
public virtual bool ModeAuto {get; set;}
C++/CLI 
public:
virtual property bool ModeAuto {
   bool get();
   void set (    bool value);
}

Remarks

Automatic mode selection is only supported on some hardware. Use IsSupported("ModeAuto") to determine whether the connected hardware supports it. The value can be set at any time, including while disconnected; it is coerced to false whenever the hardware configuration connects or is edited and the connected hardware does not support automatic mode selection.

For most cases when auto is supported and in auto mode it is a situation where the hardware may be shared with other applications and when in auto it will use the state of the mode the hardware was in at the time this application connected to the hardware.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

Minimum Software Version Requirement: Keysight 89600 VSA Ver 31.00

See Also