| Visual Basic (Declaration) | |
|---|---|
Public Overridable Property Mode As CalibrationMode | |
| C# | |
|---|---|
public virtual CalibrationMode Mode {get; set;} | |
| C++/CLI | |
|---|---|
public: virtual property CalibrationMode Mode { CalibrationMode get(); void set ( CalibrationMode value); } | |
Selectable modes are only meaningful when the connected hardware supports them. Use ValidValues<Mode>("Mode") to get the modes the current hardware supports. The set is captured when the hardware configuration connects and is retained while disconnected; before the first connection it contains only the current value. On hardware that only supports traditional calibration the mode is fixed at Classic; on hardware that does not support calibration at all it is CalibrationMode.NotApplicable
When ModeAuto is on, the getter reflects the mode the hardware selected (read-only), and the setter records the mode to use if ModeAuto is later turned off.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)
Minimum Software Version Requirement: Keysight 89600 VSA Ver 31.00