Keysight 89600 VSA .NET API
Correction Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : Correction Class


Glossary Item Box

User-configurable frequency converter correction and fixed equalization for logical channels.

Object Model

Correction ClassDataRegister ClassMeasurementData ClassStateDictionary Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class Correction 
   Inherits RemotableObject
   Implements IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged 
C++/CLI 
public ref class Correction abstract : public RemotableObject, IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged  

Remarks

This class has properties and methods that allow the user to apply fixed equalization to a logical channel, and also properties to compensate for the presence of an external frequency converter.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also