Keysight 89600 VSA .NET API
Correction Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : Correction Class

Glossary Item Box

The following tables list the members exposed by Correction.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyExternalConverterIFBandwidthGets or sets the maximum measurement bandwidth at the IF output of the external frequency converter.  —
Public PropertyExternalConverterIFCenterGets or sets the center frequency at the IF output of the external frequency converter.  —
Public PropertyExternalConverterRFCenterGets or sets the center frequency at the RF input of the external frequency converter.  —
Public PropertyExternalConverterSpectrumGets or sets how the external frequency converter inverts (mirrors) the spectrum around the center frequency.  —
Public PropertyFixedEqualizerRegisterGets or sets which data register supplies data to the fixed equalizer.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsExternalConverterEnabledGets or sets a value indicating whether an external down converter correction is being used.  —
Public PropertyIsFixedEqualizerEnabledGets or sets a value indicating whether the fixed equalizer is enabled.  —
Public PropertyIsFixedEqualizerInvertedGets or sets a value indicating whether the fixed equalization data is mathematically inverted before being applied.  —
Public PropertyIsFixedEqualizerRelativeGets a value indicating whether the fixed equalizer maps frequency relatively.  —
Public PropertyTimeCoefficientsGenerationEnabledGets or sets a value indicating whether to generate time coefficients for the fixed equalizer.  29.00
Public PropertyTimeCoefficientsLeftLengthGets or sets the desired number of samples to the left of the center of the time coefficients.  29.00
Public PropertyTimeCoefficientsRightLengthGets or sets the desired number of samples to the right of the center of the time coefficients.  29.00
Public PropertyTimeCoefficientsSampleRateGets or sets the desired sample rate for the time coefficients.  29.00
Public PropertyTimeCoefficientsSampleRateAutoGets or sets a value indicating whether the sample rate for the time coefficients is automatically determined.  29.00
Public PropertyTimeCoefficientsTruncationEnabledGets or sets a value indicating whether to truncate the time coefficients to a desired length.  29.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodValidateRegisterUsed to check if a data register can be used for fixed equalization.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also