Keysight 89600 VSA .NET API
IsFixedEqualizerEnabled Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Correction Class : IsFixedEqualizerEnabled Property


Glossary Item Box

Gets or sets a value indicating whether the fixed equalizer is enabled.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsFixedEqualizerEnabled As Boolean
C# 
public abstract bool IsFixedEqualizerEnabled {get; set;}
C++/CLI 
public:
abstract property bool IsFixedEqualizerEnabled {
   bool get();
   void set (    bool value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also