Keysight 89600 VSA .NET API
Display Class
Members  See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : Display Class


Glossary Item Box

The Display class contains objects/methods that control the visual aspects of the application.

Object Model

Display ClassDisplayFontInfo StructurePrinter ClassResultCollection ClassResult ClassResult ClassTraceCollection ClassTrace ClassGraph ClassMarkerCollection ClassMeasurementData ClassSpectrogram ClassTrace ClassGraph ClassMarkerCollection ClassMeasurementData ClassSpectrogram ClassTrace ClassGraph ClassMarkerCollection ClassMeasurementData ClassSpectrogram ClassViewCollection ClassView Class

Syntax

Visual Basic (Declaration) 
Public MustInherit Class Display 
   Inherits RemotableObject
   Implements IPropertyInfo, IPropertyInfo2, IRemoteNotifyPropertyChanged, IRemoteNotifyPropertyInfoChanged 

Remarks

The objects include the Traces collection, the Views collection (used for printing), and the Printer. The properties include fonts, colors, and themes used by the display.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also