Keysight 89600 VSA .NET API
Display Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : Display Class

Glossary Item Box

The following tables list the members exposed by Display.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyColorCountGets the number of colors used by the Color methods.  —
Public PropertyFontCountGets the number of fonts used by the Font methods.  —
Public PropertyIsDialogAboveMainWindowGets or sets a value indicating whether property dialogs are always above the main window.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyIsFixedSizePropertyDialogsGets or sets a value indicating whether property dialogs are fixed size.  —
Public PropertyLayoutStringGets or sets the application window layout.  —
Public PropertyMapUserColorNamesGets or sets all the colors (as strings) in the spectrogram user color map.  —
Public PropertyMapUserDefaultColorNamesGets the default colors (as strings) for a spectrogram user color map.  —
Public PropertyPrinterGets the Printer object.  —
Public PropertyResultsGets the results collection (For internal use only)  —
Public PropertyThemeGets or sets the color theme to be applied to all windows.  —
Public PropertyTraceColorCountGets the number of traces (20) for which colors are remembered.  —
Public PropertyTracesGets the TraceCollection object.  —
Public PropertyViewsGets the ViewCollection collection.  —
Public PropertyWindowScaleFactorGets or sets the scaling factor applied to all window contents.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodColorOverloaded. Get the color (as a string) for the color index.  —
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodFontOverloaded. Get the font for the font index.  —
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetDataBurstColorGet the color (as a string) for the color index.  24.20
Public MethodGetDataBurstColorsGet the data burst colors (as a string array).  24.20
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodIsColorByTraceReturns true if this color index can be different for each trace.  —
Public MethodPresetPreset the display properties to a default state.  —
Public MethodRecallFileRecall the display attributes from a file.  —
Public MethodRecallLayoutRecall the application window layout from a file.  —
Public MethodRecallMapUserColorsRecall the spectrogram user color map colors from a file.  —
Public MethodSaveFileSave the display attributes to a file.  —
Public MethodSaveLayoutSave the application window layout to a file.  —
Public MethodSaveMapUserColorsSave the spectrogram user color map colors to a file.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also