Keysight 89600 VSA .NET API
Color Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Display Class : Color Method


Glossary Item Box

Get the color (as a string) for the color index.

Overload List

OverloadDescription
Color(DisplayColor,Int32)Get the color (as a string) for the color index.  
Color(DisplayColor,Int32,String)Set the color (as a string) for the color index.  

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also