Keysight 89600 VSA .NET API
IsColorByTrace Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Display Class : IsColorByTrace Method


colorIndex
The color index.

Glossary Item Box

Returns true if this color index can be different for each trace.

Syntax

Visual Basic (Declaration) 
Public MustOverride Function IsColorByTrace( _
   ByVal colorIndex As DisplayColor _
) As Boolean
C# 
public abstract bool IsColorByTrace( 
   DisplayColor colorIndex
)
C++/CLI 
public:
abstract bool IsColorByTrace( 
   DisplayColor colorIndex
) 

Parameters

colorIndex
The color index.

Return Value

Whether the code can be different for each trace.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also