Keysight 89600 VSA .NET API
IsDialogAboveMainWindow Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Display Class : IsDialogAboveMainWindow Property


Glossary Item Box

Gets or sets a value indicating whether property dialogs are always above the main window.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IsDialogAboveMainWindow As Boolean
C# 
public abstract bool IsDialogAboveMainWindow {get; set;}
C++/CLI 
public:
abstract property bool IsDialogAboveMainWindow {
   bool get();
   void set (    bool value);
}

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also