Keysight 89600 VSA .NET API
SaveFile Method
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > Display Class : SaveFile Method


fileName
The file name.

Glossary Item Box

Save the display attributes to a file.

Syntax

Visual Basic (Declaration) 
Public MustOverride Sub SaveFile( _
   ByVal fileName As String _
) 
C# 
public abstract void SaveFile( 
   string fileName
)
C++/CLI 
public:
abstract void SaveFile( 
   String^ fileName
) 

Parameters

fileName
The file name.

Remarks

These are the same attributes affected by Preset.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also