| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property IOffset As Double | |
| C# | |
|---|---|
public abstract double IOffset {get; set;} | |
Adjusts the DC offset of the I signal before entering the instrument's port. Removing the DC offset allows the instrument to correctly process the entire signal. The DC offset values are a percentage relative to the RMS waveform voltage being played out of the ARB.
The IsSupported("IOffset") method can be used to determine whether this property is supported with the current Source.SelectedHardware and source logical channel type.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)