Keysight 89600 VSA .NET API
IQOutput Class Members
See Also  Properties  Methods  Events
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace : IQOutput Class

Glossary Item Box

The following tables list the members exposed by IQOutput.

Public Properties

 NameDescriptionMinimum SW Version
Public PropertyAdjustmentsEnabledGets or sets a value indicating whether I/Q output adjustments are applied.  —
Public PropertyIOffsetGets or sets the DC offset in percent applied to the I output.  —
Public PropertyIQDelayGets or sets a delay in seconds on both I and Q that adjusts the phase of both with respect to triggers and markers.  —
Public PropertyIQGainGets or sets the I/Q gain adjustment in dB.  —
Public PropertyIQPhaseGets or sets the I/Q phase adjustment in degrees.  —
Public PropertyIQSkewGets or sets relative time delay between I and Q signals in seconds.  —
Public PropertyIsDisposedGets a value indicating whether the object has been disposed. If an object has been disposed any attempt to use it will lead to an ObjectDisposedException being thrown. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public PropertyQOffsetGets or sets the DC offset in percent applied to the Q output.  —
Public PropertyQuadratureAngleGets or sets the quadrature angle adjustment in degrees.  —
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Methods

 NameDescriptionMinimum SW Version
Public MethodCreateObjRefCreates an object that contains all the relevant information required to generate a proxy used to communicate with a remote object. (Inherited from System.MarshalByRefObject)—
Public MethodForceRebuildKeyMapThis method is used to force a refresh of the key map. This is necessary in cases where the key mappings to the API objects change. This can happen when the index of an item within a collection is reflected in the key name, and an item is removed from the middle of a collection. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public MethodGetLifetimeServiceRetrieves the current lifetime service object that controls the lifetime policy for this instance. (Inherited from System.MarshalByRefObject)—
Public MethodInitializeLifetimeServiceObtains a lifetime service object to control the lifetime policy for this instance. (Inherited from Agilent.SA.Vsa.RemotableObject)—
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

Public Events

 NameDescriptionMinimum SW Version
Public EventPropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventPropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyChangedOccurs when a property value changes. (Inherited from Agilent.SA.Vsa.RemotableObject)—
Public EventRemotePropertyInfoChangedOccurs when secondary information about a property, such as limits, changes. (Inherited from Agilent.SA.Vsa.RemotableObject)14.00
‡ This is the minimum 89600 VSA software version level needed to use this member.
Top

See Also