Keysight 89600 VSA .NET API
IQDelay Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > IQOutput Class : IQDelay Property


Glossary Item Box

Gets or sets a delay in seconds on both I and Q that adjusts the phase of both with respect to triggers and markers.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IQDelay As Double
C# 
public abstract double IQDelay {get; set;}
C++/CLI 
public:
abstract property double IQDelay {
   double get();
   void set (    double value);
}

Remarks

A positive value delays I and Q.

The IsSupported("IQDelay") method can be used to determine whether this property is supported with the current Source.SelectedHardware and source logical channel type.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also