| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property IQGain As Double | |
| C# | |
|---|---|
public abstract double IQGain {get; set;} | |
Adjusts the ratio of I to Q while preserving the composite, vector magnitude. Adding Gain (+x dB) to the signal increases the I component and decreases the Q component proportionally. Reducing Gain (-x dB) decreases the I component and increases the Q component proportionally.
The IsSupported("IQGain") method can be used to determine whether this property is supported with the current Source.SelectedHardware and source logical channel type.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)