Keysight 89600 VSA .NET API
IQPhase Property
See Also 
Agilent.SA.Vsa.Interfaces Assembly > Agilent.SA.Vsa Namespace > IQOutput Class : IQPhase Property


Glossary Item Box

Gets or sets the I/Q phase adjustment in degrees.

Syntax

Visual Basic (Declaration) 
Public MustOverride Property IQPhase As Double
C# 
public abstract double IQPhase {get; set;}
C++/CLI 
public:
abstract property double IQPhase {
   double get();
   void set (    double value);
}

Remarks

Adjusts the absolute phase of the internal I/Q channel by rotating both I and Q, thus adjusting the relative phase of the RF carrier.

The IsSupported("IQPhase") method can be used to determine whether this property is supported with the current Source.SelectedHardware and source logical channel type.

Requirements

Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)

See Also