| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property IQSkew As Double | |
| C# | |
|---|---|
public abstract double IQSkew {get; set;} | |
Skew is typically used either to create impairments, or to reduce error vectors on large bandwidth signals.
Adjust I/Q Skew can correct a relative time delay between the I and Q signals. The different signal paths traveled by the I and Q signals result in time delay differences that show up as an EVM error in large bandwidth modulated signals. Adding an equal and opposite time delay (skew) in the I/Q signals during baseband generation eliminates the time delay error, correcting for any delays in signals that are generated in the internal baseband generator.
The IsSupported("IQSkew") method can be used to determine whether this property is supported with the current Source.SelectedHardware and source logical channel type.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)