| Visual Basic (Declaration) | |
|---|---|
Public MustOverride Property QuadratureAngle As Double | |
| C# | |
|---|---|
public abstract double QuadratureAngle {get; set;} | |
Offsets the phase of the Q signal relative to the phase of the I signal in degrees.
The IsSupported("QuadratureAngle") method can be used to determine whether this property is supported with the current Source.SelectedHardware and source logical channel type.
Target Platforms: Windows 11 Professional or Enterprise; Windows 10 Professional, Enterprise, or Education (64-bit)